MK64FX512 : VREF_OUT voltage drift

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64FX512 : VREF_OUT voltage drift

Jump to solution
1,689 Views
koichisakagami
Contributor II

Dear community,

We consider the VREF_OUT voltage drift.

In DataSheet Table 36. VREF full-range operating behaviors ,
It is described that VOUT = 1.198 V (max);( Vout Voltage reference output with factory trim at nominal VDDA and temperature= 25 °C ) .

  Vtdrift = 15mV ( max ) ;(Vmax -Vmin across the full temperature range)
  Vvdrift = 2mV ( max );(Vmax -Vmin across the full voltage range)

Next,
Table 38. VREF limited-range operating behaviors ,
It is described that VOUT = 1.225 V (max);temperature= 0 ~ 50 °C

We calculated a max case value for voltage drift.
1.198 + 0.015 + 0.002 = 1.215

[Question]
Why  is the max case value ( we  calculated) smaller than Table 38 value ?
1.215 < 1.225

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,528 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

It seems that there is discrepancy as you said. I seems that  that the Vtdrift spec has issue, some data sheet says that the maximum of Vtdrift is 80mV instead of 15mV. You can download the data sheet of the other Kinetis K family.

BR

Xiangjun Rong

View solution in original post

0 Kudos
Reply
1 Reply
1,529 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

It seems that there is discrepancy as you said. I seems that  that the Vtdrift spec has issue, some data sheet says that the maximum of Vtdrift is 80mV instead of 15mV. You can download the data sheet of the other Kinetis K family.

BR

Xiangjun Rong

0 Kudos
Reply