MK64FX SRAM size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK64FX SRAM size

1,786件の閲覧回数
isaotakashima
Contributor IV

I want to make sure the SRAM size of the MK64FX512Vxx12 family.

According to 3.5.3.1 SRAM sizes on page 109 of reference manual of the MK64,  the SRAM size of the MK64FX512Vxx12 is 192KB.

However, according to Kinetis K series selector guide, the SRAM size of the MK64FX512Vxx12 is 256KB.

Which information is correct?

Please reply as soon as possible.

Best regards,

Takashima

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,542件の閲覧回数
alexpimenov
Contributor I

Hi,isaotakashima ,

Were you able to  access all 256KB of SRAM on K64FX512?  

0 件の賞賛
返信

1,542件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Isao Takashima 

It's a documentation issue to have this inconsistency. K64FX512 has a SRAM memory size of 256 KB. 64 KB are the SRAM_L memory and 192 KB for the SRAM_U.

Sorry for the misleading information you found.


Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信