MK64FN1M0VLL12 Reference Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK64FN1M0VLL12 Reference Manual

ソリューションへジャンプ
5,598件の閲覧回数
shauldorf
Contributor V

FRDM-K64F uses MK64FN1M0VLL12 processor.

In reference manual different register configurations referee to chip-specific configuration.

For example PORTx PCRn (page 283)  in K64 Sub-Family Reference Manual

Document Number: K64P144M120SF5RM Rev. 2,
January 2014

ReferencManual.jpg
Where this chip-specific can be found and downloaded ?

0 件の賞賛
返信
1 解決策
2,337件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi shaul dorf,

    Actually, if the chip using the same reference manual ,then the register configuration is the same.

84.jpg

     From the above picture, you will get that MK64FN1M0VLL12 should refer to this document, the reference manual which you are referring is correct.

    If you want to choose the MUX, and don't know which alternative chip-specific mean, please refer to page 246, 10.3.1 K64 Signal Multiplexing and Pin Assignments, here you will get the detail ALTn function.

85.jpg

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,338件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi shaul dorf,

    Actually, if the chip using the same reference manual ,then the register configuration is the same.

84.jpg

     From the above picture, you will get that MK64FN1M0VLL12 should refer to this document, the reference manual which you are referring is correct.

    If you want to choose the MUX, and don't know which alternative chip-specific mean, please refer to page 246, 10.3.1 K64 Signal Multiplexing and Pin Assignments, here you will get the detail ALTn function.

85.jpg

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信