MK64FN1M0VLL12 Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64FN1M0VLL12 Reference Manual

Jump to solution
5,607 Views
shauldorf
Contributor V

FRDM-K64F uses MK64FN1M0VLL12 processor.

In reference manual different register configurations referee to chip-specific configuration.

For example PORTx PCRn (page 283)  in K64 Sub-Family Reference Manual

Document Number: K64P144M120SF5RM Rev. 2,
January 2014

ReferencManual.jpg
Where this chip-specific can be found and downloaded ?

0 Kudos
Reply
1 Solution
2,346 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi shaul dorf,

    Actually, if the chip using the same reference manual ,then the register configuration is the same.

84.jpg

     From the above picture, you will get that MK64FN1M0VLL12 should refer to this document, the reference manual which you are referring is correct.

    If you want to choose the MUX, and don't know which alternative chip-specific mean, please refer to page 246, 10.3.1 K64 Signal Multiplexing and Pin Assignments, here you will get the detail ALTn function.

85.jpg

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,347 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi shaul dorf,

    Actually, if the chip using the same reference manual ,then the register configuration is the same.

84.jpg

     From the above picture, you will get that MK64FN1M0VLL12 should refer to this document, the reference manual which you are referring is correct.

    If you want to choose the MUX, and don't know which alternative chip-specific mean, please refer to page 246, 10.3.1 K64 Signal Multiplexing and Pin Assignments, here you will get the detail ALTn function.

85.jpg

Wish it helps you!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply