MK64F512x chip could not be programmed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64F512x chip could not be programmed.

Jump to solution
1,997 Views
chhsu0229
Contributor II

I am working on MK64F512x chip. However, it could not be re-programmed and connected again.How can I fix this untinted behavior?

 

The following shows the debug message from J-Link tool.

- Executing default behavior previously saved in the registry.
- Device will be unsecured now.
- Timeout while unsecuring device. Erase never starts.
- Found SW-DP with ID 0x2BA01477
- DPIDR: 0x2BA01477
- Scanning AP map to find all available APs
- AP[2]: Stopped AP scan as end of AP map has been reached
- AP[0]: AHB-AP (IDR: 0x24770011)
- AP[1]: JTAG-AP (IDR: 0x001C0000)
- Iterating through AP map to find AHB-AP to use
- AP[0]: Skipped. Could not read CPUID register
- AP[1]: Skipped. Not an AHB-AP
- ERROR: Could not find core in Coresight setup
code -1
- ERROR: Failed to connect.
Could not establish a connection to target.

0 Kudos
Reply
1 Solution
1,990 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer the answer in Communication error while accessing MDM-AP.

Hope it helps.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,991 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer the answer in Communication error while accessing MDM-AP.

Hope it helps.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply