MK60DN512VLL10 header file no SRSL for reset cause

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512VLL10 header file no SRSL for reset cause

Jump to solution
1,364 Views
CiaranMacA_hkc
Contributor III

The latest version of my header for this part "MK60D10.h" does not seem to have access to reset cause register SRSL. Indeed the same for the RM. For other versions of the K series you can read reset cause from SRSL.

Extract from header version:

** Reference manual:K60P144M100SF2V2RM Rev. 2, Jun 2012
** Version:         rev. 1.8, 2013-06-24

I need to read back the reset cause. Any ideas?

Thanks

Ciarán Mac Aonghusa.

0 Kudos
Reply
1 Solution
1,232 Views
perlam_i_au
Senior Contributor I

The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:

View solution in original post

0 Kudos
Reply
2 Replies
1,233 Views
perlam_i_au
Senior Contributor I

The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:

0 Kudos
Reply
1,232 Views
CiaranMacA_hkc
Contributor III

Thank you Perla Andrea.

0 Kudos
Reply