MK60DN256 CPUID 0x410FC24 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MK60DN256 CPUID 0x410FC24 ?

跳至解决方案
3,340 次查看
nico547845
Contributor I

Hello

I Have been using MK60DN256VLL for years and the CPUID during programming has always been 0x410FC241.

We have some chips from a different source and the CPUID is now 0x410FC240. Our code doesn't seem to run, how can I decode this CPUID to understand what is going on ?

 

Thanks

0 项奖励
回复
1 解答
3,334 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nico547845,

CPUID Base Register
[3:0] Revision Revision number, the p value in the rnpn product revision identifier:
0x0 = Patch 0
0x1 = Patch 1

Patch 0.pngPatch 1.png

Would you please show the photo of these two MCUs? Check the part number(first line) and mask set(second line), there may some different between these two MCUs.
This is the photo of MCU on TWR-K60N512 during debug I can see the CPUID=0x410FC240

MCU photo.jpg

SCB_CPUID 0x410fc240.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,293 次查看
nico547845
Contributor I

Thank you for your help Robin, all clear now.

0 项奖励
回复
3,320 次查看
nico547845
Contributor I

Hi Robin 

The chips I have problems with are 

MK60DN256ZVLL10

4N30D

The ones that work 

MK60DN256VLL10

5N22D

 

 

0 项奖励
回复
3,303 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

AN4445 Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide will show you the difference between MK60DN256VLL10 and MK60DN256ZVLL10. The program developed for MK60DN256VLL10 cannot be run directly on MK60DN256ZVLL10 without modification.

0 项奖励
回复
3,335 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nico547845,

CPUID Base Register
[3:0] Revision Revision number, the p value in the rnpn product revision identifier:
0x0 = Patch 0
0x1 = Patch 1

Patch 0.pngPatch 1.png

Would you please show the photo of these two MCUs? Check the part number(first line) and mask set(second line), there may some different between these two MCUs.
This is the photo of MCU on TWR-K60N512 during debug I can see the CPUID=0x410FC240

MCU photo.jpg

SCB_CPUID 0x410fc240.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复