MK60 Processor Expert Generation v.s Specification for NFC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK60 Processor Expert Generation v.s Specification for NFC

3,311件の閲覧回数
henrynguyen
Contributor IV

Hello,

I am observing differences between what being configured in PE v.s. what is on the spec.

I select NFC clock to be 15 MHz.  From PE, it showed that the clock is derived from PLL and divided down.  The generated codes seems to match with the specification, but not matching with what displayed on PE.

attachments 1 showed the clock selection (derived from PLL => bus clock) and the generated codes.  Attachment 2 + 3 showed that the generated codes configured NFC SRC to be 3 which is OSC clock and NFC_CLKSEL to be 1 which is external clock.  However, this is not true.  Is there a problem with the specification?  The NFC clock measured on scope seems to be matching with what was configured by PE.

can you please clarify?  This is KDS 3.0 and KSDK 1.3.

Thanks,

Henry

0 件の賞賛
返信
1 返信

3,215件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Henry,

I have a picture of MK60 clock tree. You can find that MK60's clock tree is very flexible and complex.

K60_clktree.png

BTW, this picture is cut from MCUXpresso config tool. I think this tool is much better than Project Expert. Even if you have to build your project base on sdk1.3, it is a good tool for you to refer to.

Regards

0 件の賞賛
返信