[MK40DX128VMD10] Flash memory size is different.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MK40DX128VMD10] Flash memory size is different.

ソリューションへジャンプ
2,597件の閲覧回数
waynejeong
Contributor II

Hello NXP

The flash memory size of operating feature on the NXP portal and flash memory size on datasheet are different.

I believe the value on datasheet is correct but I need your confirm.

Please see following pictures and let me know which one is correct.

- https://www.nxp.com/part/MK40DX128VMD10#/

waynejeong_0-1639652918192.jpeg

- datasheet

waynejeong_1-1639653031149.jpeg

Thank you.

 

0 件の賞賛
返信
1 解決策
2,585件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @waynejeong 

 

Many thanks for your patience and hoping you are well.

 

Effectively, the flash memory size from operating features on the NXP portal have an error. The correct flash memory size for this part number MK40DX128VMD10 is 128kB on Program flash memory size.

Thanks a lot for letting me know. If you have more questions, feel free to ask for us.

 

Sincerely,

Pablo Avalos

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,573件の閲覧回数
waynejeong
Contributor II

Dear PabloAvalos

Thank you for your answer.

 

 

0 件の賞賛
返信
2,586件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @waynejeong 

 

Many thanks for your patience and hoping you are well.

 

Effectively, the flash memory size from operating features on the NXP portal have an error. The correct flash memory size for this part number MK40DX128VMD10 is 128kB on Program flash memory size.

Thanks a lot for letting me know. If you have more questions, feel free to ask for us.

 

Sincerely,

Pablo Avalos

0 件の賞賛
返信
2,533件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hey, @waynejeong 

 

Hoping you are excellent and having happy holidays.

 

Just adding, the official NXP Portal might be confusing, because it considers Flash Memory such as real Flash Memory + FlexNVM (Non-Volatile Flash Memory), and the part number that you mentioned has a FlexNVM of 128KB, so together the regular flash and FlexNVM, form 256KB.

Please check this pdf on page 18 where you are able to see this information:

https://www.nxp.com/docs/en/product-selector-guide/KINETISKMCUSELGD.pdf

Let me know if you have more questions.

 

Regards.

Pablo Avalos.

0 件の賞賛
返信