MK20 power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20 power consumption

1,243件の閲覧回数
sreeramadhanala
Contributor I

Dear sir,

I am beginner for  Kinetis  Controllers.

I am using MK20dx128vlh5 for my application.

But , I  am not understand supply current of "MK20dx128vlh5"  !

I saw two variants in datasheet as shown in below

1.pastedImage_2.png

2.pastedImage_3.png

But practically i observed  "2" condition.(I observed "18.9" mA).

Please clarify , "1" condition requirements ? & Which one is real supply current ?

Thank you.

Dhanalakshmi

ラベル(1)
0 件の賞賛
返信
1 返信

1,147件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Dhanalakshmi,

There are two Application Note about the power consumption of Kinetis MCU.
AN4470 Using Low Power modes on Kinetis family
AN4503 Power Management for Kinetis MCUs When and how to use Kinetis low-power modes


The current of MCU is depend on how you use the MCU.
"1" 155 mA is the maximum current of MCU.
There are several low power modes for Kinetis MCU, "2" Run mode is one of them.

 

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信