MK20 power consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20 power consumption

1,237 Views
sreeramadhanala
Contributor I

Dear sir,

I am beginner for  Kinetis  Controllers.

I am using MK20dx128vlh5 for my application.

But , I  am not understand supply current of "MK20dx128vlh5"  !

I saw two variants in datasheet as shown in below

1.pastedImage_2.png

2.pastedImage_3.png

But practically i observed  "2" condition.(I observed "18.9" mA).

Please clarify , "1" condition requirements ? & Which one is real supply current ?

Thank you.

Dhanalakshmi

Labels (1)
0 Kudos
Reply
1 Reply

1,141 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Dhanalakshmi,

There are two Application Note about the power consumption of Kinetis MCU.
AN4470 Using Low Power modes on Kinetis family
AN4503 Power Management for Kinetis MCUs When and how to use Kinetis low-power modes


The current of MCU is depend on how you use the MCU.
"1" 155 mA is the maximum current of MCU.
There are several low power modes for Kinetis MCU, "2" Run mode is one of them.

 

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply