MK20: Internal Clock tolerance Query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20: Internal Clock tolerance Query

2,350 次查看
pj0585
Contributor IV
Hi,
I'm trying to see if I can use internal fast clock of 4Mhz (MK20DNxxxVLL10) instead of using external crystal. I could not find tolerance on the internal clock in datasheet over temperature, life or any other factor.
I want to see if I can use it for USB and CAN buses clock source.
Any inputs on the above will be helpful.
Regards, Pj
标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

2,203 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Prasant J,

  1,Internal 4Mhz IRC range is:

pastedImage_1.png

So, it is not very accurate, even you use it, you can't use the PLL or FLL to double it.

pastedImage_2.png

2. I want to see if I can use it for USB and CAN buses clock source.

If you are using the USB and CAN bus, there's no doubt, you can't use internal IRC, no matter slow or the faster.

You must use the external crystal as the USB and CAN clock source. USB need 48Mhz clock, CAN also need the accurate clock source.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,203 次查看
mjbcswitzerland
Specialist V

Hi Pj

The specifications of the fast clock is something that seems to be missing in the data sheets of all Kinetis parts, however it is not needed to answer your questions.

For USB you have no choice but to use a suitably accurate crystal (such as 8MHz). And for CAN the crystal source is always recommended (lowest jitter) as clock too.

Regards

Mark