MK10DN512Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,864件の閲覧回数
赵壮钦
Contributor III

你好!

MK10DN512ZVMD10 Mask Set Errata 2N22D, 4N22D or 5N22D?

0 件の賞賛
返信
1 解決策
1,853件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 赵壮钦,

The maskset is on the second line of the MCU surface, you should be able to see it directly. According to the information of AN4445, ‘Z’ character: INITIAL Production mask set should be 4N30D.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,854件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 赵壮钦,

The maskset is on the second line of the MCU surface, you should be able to see it directly. According to the information of AN4445, ‘Z’ character: INITIAL Production mask set should be 4N30D.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信