MK10DN512Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10DN512Z

Jump to solution
1,870 Views
赵壮钦
Contributor III

你好!

MK10DN512ZVMD10 Mask Set Errata 2N22D, 4N22D or 5N22D?

0 Kudos
Reply
1 Solution
1,859 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 赵壮钦,

The maskset is on the second line of the MCU surface, you should be able to see it directly. According to the information of AN4445, ‘Z’ character: INITIAL Production mask set should be 4N30D.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,860 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 赵壮钦,

The maskset is on the second line of the MCU surface, you should be able to see it directly. According to the information of AN4445, ‘Z’ character: INITIAL Production mask set should be 4N30D.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply