MFS_READ_FAULT error when SD card mount on K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFS_READ_FAULT error when SD card mount on K60

3,130件の閲覧回数
vallinaths
Contributor II

Platform : MQX 4.0.2

controller : K60

USing the example code of SD card drom path /mfs/examples/sd card .

dev_handle1 = fopen("sdcard:", 0);

if ( dev_handle1 == NULL ) {

printf("\nUnable to open SD card device");

_task_block();

}

/* Install MFS: */

error_code = _io_mfs_install(dev_handle1, "a:", 0);

if ((error_code != MFS_NO_ERROR) &&

(error_code != MFS_NOT_A_DOS_DISK)) {

printf("FATAL error while initializing: \n");

_mqx_exit(1);

} else {

printf("Initialized MFS1%s\n");

}

//open filse system

file_handle=fopen("a:",NULL);

The task is getting a error of MFS READ fault , checked the user guide of MFS which means low level driver is not respondin properly . so please let me know anybody faced same issue how to resolve it

is they any CLOCK issue which is going on SDHC CLK pin .

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,771件の閲覧回数
jieli
Contributor I

have you solved this problem? I met the same issue as you.

0 件の賞賛
返信

2,771件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Are you using a Freescale board (twrk60d100m, twrk60f120m or twrk60n512) ?

Could you please attach the complete code that you modified?


Have a great day,
Regards
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,771件の閲覧回数
vallinaths
Contributor II

Hi soledad

   We are using twrk60d100m tower kit , also we are trying on customised board using K60 with SD card support

if (last != inserted)

        {

            last = inserted;              

            if (inserted)

            {

                _time_delay (200);

                /* Open the device which MFS will be installed on */

                sdcard_handle = fopen("sdcard:", 0);

                if (sdcard_handle == NULL)                {

                    printf("Unable to open SD card device.\n");

                    continue;

                }

                /* Set read only flag as needed */

                param = 0;

                if (readonly)

                {

                    param = IO_O_RDONLY;

                }

                if (IO_OK != ioctl(sdcard_handle, IO_IOCTL_SET_FLAGS, (char_ptr) &param))

                {

                    printf("Setting device read only failed.\n");

                    continue;

                }

                /* Install partition manager over SD card driver */

                error_code = _io_part_mgr_install(sdcard_handle, partman_name, 0);

                if (error_code != MFS_NO_ERROR)

                {

                    printf("Error installing partition manager: %s\n", MFS_Error_text((uint_32)error_code));

                    continue;

                }

                /* Open partition */

                partition_handle = fopen(partition_name, NULL);

                if (partition_handle != NULL)

                {

                    printf("Installing MFS over partition...\n");                   

                    /* Validate partition */

                    error_code = _io_ioctl(partition_handle, IO_IOCTL_VAL_PART, NULL);

                    if (error_code != MFS_NO_ERROR)

                    {

                        printf("Error validating partition: %s\n", MFS_Error_text((uint_32)error_code));

                        printf("Not installing MFS.\n");

                        continue;

                    }

                    /* Install MFS over partition */

                    error_code = _io_mfs_install(partition_handle, filesystem_name, 0);

                    if (error_code != MFS_NO_ERROR)

                    {

                        printf("Error initializing MFS over partition: %s\n", MFS_Error_text((uint_32)error_code));

                    }

                } else {

                    printf("Installing MFS over SD card driver...\n");              

                    /* Install MFS over SD card driver */

                    error_code = _io_mfs_install(sdcard_handle, filesystem_name, (_file_size)0);

                    if (error_code != MFS_NO_ERROR)

                    {

                        printf("Error initializing MFS: %s\n", MFS_Error_text((uint_32)error_code));

                    }

                }

                /* Open file system */

                if (error_code == MFS_NO_ERROR) {

                    filesystem_handle = fopen(filesystem_name, NULL);

                    error_code = ferror(filesystem_handle);

                    if (error_code == MFS_NOT_A_DOS_DISK)

                    {

                        printf("NOT A DOS DISK! You must format to continue.\n");

                    }

                    else if (error_code != MFS_NO_ERROR)

                    {

                        printf("Error opening filesystem: %s\n", MFS_Error_text((uint_32)error_code));

                        continue;

                    }

                    printf ("SD card installed to %s\n", filesystem_name);

                    if (readonly)

                    {

                        printf ("SD card is locked (read only).\n");

                    }

                }

            }

            else

            {

                /* Close the filesystem */

            if ((filesystem_handle != NULL) && (MQX_OK != fclose(filesystem_handle)))

                {

                    printf("Error closing filesystem.\n");

                }

            filesystem_handle = NULL;

                /* Uninstall MFS  */

                error_code = _io_dev_uninstall(filesystem_name);

                if (error_code != MFS_NO_ERROR)

                {

                    printf("Error uninstalling filesystem.\n");

             

Actually disabled partion manager code part and  tried installing the MFS on SD card driver . when we opeen the filesystem getting an error " MFS read fault"

please let us know what need to be debugged.

0 件の賞賛
返信

2,771件の閲覧回数
vallinaths
Contributor II

please suggest further

0 件の賞賛
返信