MCUexpresso Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUexpresso Reset

1,581件の閲覧回数
MWMinor
Contributor V

I am trying to migrate from Codewarrior to MCUexpresso - so please excuse the simple question.

The Codewarrior  IDE included a really useful RESET function/button when running debug. I can't see anything similar in the MCUExpresso IDE - but it must be there surely....?

Can anyone assist..?

thanks

 

Ken

0 件の賞賛
返信
2 返答(返信)

1,575件の閲覧回数
ErichStyger
Specialist I

There is the 'Restart' button

ErichStyger_0-1665420795932.pngErichStyger_0-1665420795932.png

It does kind of the same. The reason is that each debug probe/connection might handle the 'reset' or 'restart' differently.

For example in the LinkServer connection you could fine tune the reset behaviour:

ErichStyger_1-1665420932662.pngErichStyger_1-1665420932662.png

 

I hope this helps,

Erich

0 件の賞賛
返信

1,569件の閲覧回数
MWMinor
Contributor V

Hi Erich

Many thanks for getting back to me and understood..

(Now all I have to figure out is where to find some examples suitable for the TWR-K53N512 board)

Ken

0 件の賞賛
返信