MCUXpresso Config Tools not working for KW37/38/39 SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Config Tools not working for KW37/38/39 SDK

913 次查看
m3
Contributor II

Is there actually any way to configure a SDK(2.6.9) for the KW38? I tried every possilbe SDK version, downloaded from inside and outside the MCUXpresso but none of them will work with the MCUX Config Tools.

 

 

0 项奖励
回复
1 回复

902 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

You can refer this topic.

https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Config-tools-not-opening-for-FRDM-KW38-Board-...

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复