MCU Temperature Reading Errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU Temperature Reading Errors

1,340件の閲覧回数
dluks
Contributor I

We use a PIT and DMA to scan a number of ADC channels ever ms on a KV31. The ADC clock is 10 Mhz (MCU clock divided by 8). On occasion, post a reboot, the single ended temperature reading from ADC0 will be stuck at 25 C or on rare occasion report roughly 10 C below the actual measured temperature. All other voltages on that ADC appear to be normal.

Has anyone had an issue like this?

Thanks,

Dave

ラベル(1)
0 件の賞賛
返信
1 返信

1,249件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Have you done anything of ADC Calibration? As the manual mentioned:

The ADC contains a self-calibration function that is required to achieve the specified accuracy.
Calibration must be run, or valid calibration values written, after any reset and before a conversion is initiated.
0 件の賞賛
返信