MCU Recovery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU Recovery

2,405 Views
LArmstrong1985
Contributor III

Hi,

I've a problem with my board so I am no longer able to program it.

I think the chip is locked. The problem arose after I tried uploading an example for a demo board with a slightly different chip than mine. Specifically, my board has the chip MK22FN1M0xxx12 while the example was for the FRDMK22 board that mounts the chip MK22FN512xxx12. Could this be the problem? I thought there was a protection mechanism in the case.

How can I fix and reset the chip? As a programmer I am using the LPC-LINK v1.3

Labels (1)
0 Kudos
Reply
4 Replies

2,306 Views
nxf56274
NXP Employee
NXP Employee

Hi,

If you think your board was locked, use jlink commander is the only way to recover it. If the your LPC link was't be viewed ,you should try other Jlink.I use the LPC-link2. If you want to download the code to different board, you have to modify the linker file. If not, the program won't work. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,306 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Do you try the jlink commander to unlock the device?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,306 Views
LArmstrong1985
Contributor III

No,

because the LPC-Link v1.3 inside the LPCxpresso Board is not viewed by

USB on J-Link Commander.

Can I use another Kinetis board with Segger J-link bootloader in this case?

Thank you very much

Fabio

0 Kudos
Reply

2,306 Views
LArmstrong1985
Contributor III

I'm having the same problem with another board.

If the problem is that the chip is continuously reset is possible to force it?

Do I have to connect it to GND or to VCC?

0 Kudos
Reply