MCU PKEAZ128MLK is not loaded on Codewarrior?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU PKEAZ128MLK is not loaded on Codewarrior?

3,642 Views
omarzamacona
Contributor II

Hello,

Im working with a Freescale board TRK-KEA 128, Kinetis EA MCU PKEAZ128MLK.

And when I tried to select the device into "Devices" window there is not the MCU that I have "PKEAZ128MLK" only is a similar device "SKEAZ128", could I use that MCU instead of "PKEA.." ?

If not, what do I need to do to add a new device like PKEAZ128MLK on the Codewarrior IDE?

- CodeWarrior for MCU

     Version: 10.6.4

Thanks!

Regards!

Labels (1)
0 Kudos
Reply
3 Replies

3,449 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello omar,

Yes, when you use the board of TRK-KEA128, please select the chip of "SKEAZ128" .

About the meaning of "P" and "S" , you can check it from the "

KEA128 Sub-Family Data Sheet "

pastedImage_0.png

In fact , there is no different between them about the application.

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,449 Views
omarzamacona
Contributor II

Hello Alice,

Thanks for your help, so, we could say that the main "part number" of any MCU (talking about Codewarrior) is for example: SKEAZ128, other letters and numbers do not matter, right?

Regards!

0 Kudos
Reply

3,449 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello omar,

- No, other latters also need care, for example the "MLK " indicate the 80 pin,

for the meaning of the part number you can refer to the "S9KEA128P80M48SF0.pdf"

pastedImage_1.png

- While all of the SKEAZ128 chip select the ""SKEAZ128".

After you create the PE project on CW, you can change the chip at here :

pastedImage_0.png

on the board of TRK-KEA128, the chip is :

pastedImage_2.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct   button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply