M4 Operating Temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M4 Operating Temperature

2,114 Views
sandeepkamath
Contributor I

Hi,

ARM M4 operating temperature is from -40 to 105 degC. Is there any spec or graph on temperature Vs Core clock.

Say, for example if i operate my M4 @ 40 MHz, can i stretch it to 125 degC

Thanks in advance

Sandeep

0 Kudos
Reply
1 Reply

1,976 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

NXP will launch S32K MCU (ARM Cortex M4 core) with auto level (operation range from –40 °C to +125 °C).

More detailed info, please check below link.

32-bit Automotive General Purpose MCUs|NXP 


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply