Looking for PMSM positional servo drive reference design and code examples.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for PMSM positional servo drive reference design and code examples.

3,104 Views
davidmccall
Contributor I

Hi I have found this note
Design of a PMSM Servo System Using the 56F8357 Device, Rev. 0 but it is dated 2006.

Is there anything more up to date using Kinetis V series . what I need is help with code for SMSP / BLAC servo code
A devolopment board setup would be good too.  Any suggestion greatly appreciated

0 Kudos
Reply
2 Replies

1,447 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, David

There is an application notes for your reference. You can find it from link http://cache.freescale.com/files/32bit/doc/app_note/AN4911.pdf?fpsp=1&WT_TYPE=Application%20Notes&WT...

Hope it can help you.

Best Regards

Paul

0 Kudos
Reply

1,447 Views
davidmccall
Contributor I

Thanks Paul,

There are many sensorless ap notes and reference, But for a positional servo system a sensor is required as smooth low speed response is necessary.

Most are about running fans, pumps and appliances such as washing machines.
So I 'm looking for something that is specifically for positional servo applications under motion control.

best regards,

David

0 Kudos
Reply