LPTMR0 interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPTMR0 interrupts

1,780件の閲覧回数
vinkar
Contributor III

Hello ,

This is basically an ISR doubt.

I am trying to interrupt when there is a timer overflow.

But, it never goes to the ISR. Kindly suggest some solutions pls -

#include "derivative.h" /* include peripheral declarations */

//void UART0_IRQHandler(void);

//extern void LPTimer_IRQ(void);

int main(void)

{

    int count;

    uint16_t countTemp = 0;

   

   

    asm(" CPSIE i");

   

    //asm volatile ("cpsie i");                  

    SIM_SOPT1 = 0;                                            

    SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);//PORTC_PCR1 |= PORT_PCR_MUX(1);//select RTC_CLKIN function

    PORTB_PCR8 |= 0x00000100;    // alternative pin mux selection //

    GPIOB_PDDR |= 0x00000100;    // pin direction //   

    /*

    NVIC_ICPR = 1 << (28);

    NVIC_ISER = 1 << (28);

    */

   

    SIM_SCGC5|=SIM_SCGC5_LPTMR_MASK;

      /* Reset LPTMR settings */

      SIM_SOPT1 = 0;                                            

    SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);//PORTC_PCR1 |= PORT_PCR_MUX(1);//select RTC_CLKIN function

   

      LPTMR0_CSR=0;     

      LPTMR0_CSR |= 0x00000040;

      /* Set the compare value to the number of ms to delay */     

      LPTMR0_CMR = 600;

      /* Start the timer */    

      LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;

      /* Wait for counter to reach compare value */

      while(1){

         

      }       

}

void LPTimer_IRQHandler(void){    

     //while (!(LPTMR0_CSR & LPTMR_CSR_TCF_MASK));    

          /* Disable counter and Clear Timer Compare Flag */     

          LPTMR0_CSR &= ~LPTMR_CSR_TEN_MASK;

          LPTMR0_CSR |= LPTMR_CSR_TCF_MASK;

          GPIOB_PTOR |= (1<<8);

          LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;    

    }

    

    /*

    void enable_irq (int irq)

    {

        //int div;

        /* Determine which of the NVICISERs corresponds to the irq */

        //        div = irq/32;

        //NVICICPR0 = 1 << (irq);

        /*

        switch (irq)  

        {

            case 0x0:

            NVICICPR0 = 1 << (irq);

            NVICISER0 = 1 << (irq%32);

            break;

            case 0x1:

            NVICICPR1 = 1 << (irq%32);

            NVICISER1 = 1 << (irq%32);

            break;

            case 0x2:

            NVICICPR2 = 1 << (irq%32);

            NVICISER2 = 1 << (irq%32);

            break;

        }

        */

    //}*/

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,323件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

hi karuvat,

I guess you miss TCF bit of LPTMR0_CSR. You can refer to the following.

pastedImage_0.png

0 件の賞賛
返信