can ripple mixed in power pin cause mcu resets?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can ripple mixed in power pin cause mcu resets?

1,111件の閲覧回数
wangbaode
Contributor IV

hi everybody,

can ripple mixed in power pin cause mcu(kl15z128) resets? and how many is the threshold of ripple voltage?

best regards for everyone

タグ(5)
0 件の賞賛
返信
2 返答(返信)

936件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Bao De

What is your ripple range? 0.5V? Do you enable LVD function? If yes, please check which LVD level you selected. As you know, VLVW4H max. value is 3.08V. Waiting for your response. Thanks

Best Regards

Paul

0 件の賞賛
返信

936件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The data sheet to the devices give the lowest operating voltage and I would expect that if any power supply ripple stays above that things would be OK.

In case you have resets that "may" be caused due to this, read the RCM_SRS0 register after a reset to see whether it was due to a "power on reset" or "low voltage detector" or possibly another reason.

Regards

Mark

0 件の賞賛
返信