LPFLL clock accuracy issue of MKE14Z256VLL7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPFLL clock accuracy issue of MKE14Z256VLL7

1,034 次查看
qinshengli
Contributor I

MKE14Z256VLL7 is used for our motor control board.

The crystal frequency is 4 MHz and LPFLL clock frequrncy is set to 72MHz.

The LPFLL clock is used for FlexTimer 0 (FTM0). The FTM0 is used for motor PWM control.

By testing we found that there are some LPFLL clock errors.

Three target boards are used for the test. The clock errors from 2 boards are negligible while the clock error from the 3rd one is about 0.8%.

Then the crystal is changed for the 3rd board but error is still the same.

What could be source of the clock error?

0 项奖励
回复
1 回复

954 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Qinsheng,

the LPFLL Frequency accuracy in closed loop is 1%. So you'd better do not use FLL as the clock base.

Regards

Jing

0 项奖励
回复