LOW POWER MODE for KL25Z USB MSD DEVICE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LOW POWER MODE for KL25Z USB MSD DEVICE

Jump to solution
3,379 Views
charanreddy
Contributor III

Hi,

can we use low power mode in kl25Z USB MSD ...?. If yes, then how to make the CPU to come out of Low power mode after inserting the device in to the Host.

Regards,

Charan

Labels (2)
1 Solution
3,149 Views
mjbcswitzerland
Specialist V

Hi

USB is "operational" only in RUN and WAIT modes and not in (very) low power modes.

However you can use very low power modes when you don't need USB operation and detect a USB host connection by connecting the USB +5V to a LLWU input (with suitable circuit). The device can then be woken by detecting this voltage being attached and operate in RUN/WAIT modes until it may be set back to a low power mode again.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

KL25: http://www.utasker.com/kinetis/FRDM-KL25Z.html / http://www.utasker.com/kinetis/TWR-KL25Z48M.html

LLWU: http://www.utasker.com/kinetis/LLWU.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

View solution in original post

0 Kudos
Reply
3 Replies
3,150 Views
mjbcswitzerland
Specialist V

Hi

USB is "operational" only in RUN and WAIT modes and not in (very) low power modes.

However you can use very low power modes when you don't need USB operation and detect a USB host connection by connecting the USB +5V to a LLWU input (with suitable circuit). The device can then be woken by detecting this voltage being attached and operate in RUN/WAIT modes until it may be set back to a low power mode again.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

KL25: http://www.utasker.com/kinetis/FRDM-KL25Z.html / http://www.utasker.com/kinetis/TWR-KL25Z48M.html

LLWU: http://www.utasker.com/kinetis/LLWU.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

0 Kudos
Reply
3,149 Views
charanreddy
Contributor III

Hi Mark,

Thank you very much for your quick replay.

While doing this i came across "USB Transceiver Control Register 0 (USBx_USBTRC0) " in the KL25Z data sheet. Is it required to use this register if i am fallowing the above method mentioned by you. I am a bit confused by the reading the description of the "USBx_USBTRC0" register.

Regards,

Charan

0 Kudos
Reply
3,149 Views
mjbcswitzerland
Specialist V

Hi

USBx_USBTRC0 is used to command a reset to the USB controller. It is generally used when configuring USB but won't necessarily be required to control low power operation or to recover from it. In low power mode all clocks to the USB controller will be stopped.

Regards

Mark