LLWU on KL14 problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLWU on KL14 problems

ソリューションへジャンプ
1,837件の閲覧回数
ulivinico
Contributor II

I've developed an application with KL25 by using the evaluation board FRDM that makes use of wakeup from low power mode by using LLWU_P5/PTB0. Everything works well.

Then I've ported the program to KL14 and everything works except the wakeup on that pin.

I read here:

https://community.freescale.com/message/319868#319868

that there is errors in documentation and LLWU interrupts on port B doesn't work. Is this true?

Is it not possible use the PTB0 as wakeup pin?

1 解決策
1,611件の閲覧回数
ulivinico
Contributor II

Update: The malfunction was due to an hardware problem of my board. Wakeup by LLWU pin is working on Port B as well in KL14.

So, It is not clear the documentation error reported in this discussion:

https://community.freescale.com/message/319868#319868

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,612件の閲覧回数
ulivinico
Contributor II

Update: The malfunction was due to an hardware problem of my board. Wakeup by LLWU pin is working on Port B as well in KL14.

So, It is not clear the documentation error reported in this discussion:

https://community.freescale.com/message/319868#319868

0 件の賞賛
返信