LLWU on KL14 problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLWU on KL14 problems

Jump to solution
1,840 Views
ulivinico
Contributor II

I've developed an application with KL25 by using the evaluation board FRDM that makes use of wakeup from low power mode by using LLWU_P5/PTB0. Everything works well.

Then I've ported the program to KL14 and everything works except the wakeup on that pin.

I read here:

https://community.freescale.com/message/319868#319868

that there is errors in documentation and LLWU interrupts on port B doesn't work. Is this true?

Is it not possible use the PTB0 as wakeup pin?

1 Solution
1,614 Views
ulivinico
Contributor II

Update: The malfunction was due to an hardware problem of my board. Wakeup by LLWU pin is working on Port B as well in KL14.

So, It is not clear the documentation error reported in this discussion:

https://community.freescale.com/message/319868#319868

View solution in original post

0 Kudos
Reply
1 Reply
1,615 Views
ulivinico
Contributor II

Update: The malfunction was due to an hardware problem of my board. Wakeup by LLWU pin is working on Port B as well in KL14.

So, It is not clear the documentation error reported in this discussion:

https://community.freescale.com/message/319868#319868

0 Kudos
Reply