L3GD20

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

L3GD20

2,166 次查看
omarvallecasas
Contributor III

Hi, did someone worked with L3GD20 Gyroscope on Freescale microcoutrollers? I'm having a issue when configuring. I'm using KL26Z128 by SPI0. Please if someone had a experience with these devices, could you share it?

Thanks in advance,

Omar

2 回复数

1,977 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

We don't have available L3GD20 chip example code.

Please check attached  KL25 SPI example code.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,977 次查看
omarvallecasas
Contributor III

Hi Ma Hui,

Thanks for your quick answer. I'm using KL25 SPI most likely to KL26 configuration for SPI, but it match with the one I was using. I send a 16 pulse clock signal with automatic CS to the L3GD20 (Gyro), MOSI signal is generated but MISO signal not, I only get noise. I recently buy the Gyros (10 pieces), with 22 FRDM-KL26Z just to do Sensor Fusion for motion tracking.

Regards,

Omar

0 项奖励
回复