Kwikstik Demo Lab for MQX not working weird problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kwikstik Demo Lab for MQX not working weird problem

ソリューションへジャンプ
2,142件の閲覧回数
nabeelkhan
Contributor I

Hi,

I am using K40X256VLQ100, Downloaded the Demo for MQX and trying it running over MQX 3.7 under Code Warrior 10.1 environment. I have successfully Built the kwitstik demo and more over can easily RUN and Debug it over software without error . But still the demo is not showing on the board or have not able to see anything on my SLCD . software is doing debugging and running what ever i want to do. but nothing take place over the board .however I have to connect the J-link while doing debug or Run otherwise it come up with error as it should do. so don't know where i am going wrong Please help me out

Thanks

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,026件の閲覧回数
nabeelkhan
Contributor I

i solved it ... The target task was not correctly selected

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,027件の閲覧回数
nabeelkhan
Contributor I

i solved it ... The target task was not correctly selected

0 件の賞賛
返信