Kinetis with LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,284件の閲覧回数
lyxljh
Contributor I

I'm a newbie in Tower System. Now I want to use K60 with a dot lcd in my project. I find there’s no LCD in K60 kit. I want to know if I can add TWR-LCD  to the K60 kit for development? And are there any graphic libs for use?

 

Thanks in advance.

0 件の賞賛
返信
1 解決策
5,301件の閲覧回数
freegeek
Contributor III

Yes, you can use the K60 with the tower LCD module and drive it over the flexbus interface, have a look at the demo video here of the alpha s/w http://www.youtube.com/watch?v=FogsMTp1-Mc

 

There is a free GUI driver called eGUI which will be released for the Kinetis in the next month or so, more info here http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EGUI&fsrch=1&sr=3

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,302件の閲覧回数
freegeek
Contributor III

Yes, you can use the K60 with the tower LCD module and drive it over the flexbus interface, have a look at the demo video here of the alpha s/w http://www.youtube.com/watch?v=FogsMTp1-Mc

 

There is a free GUI driver called eGUI which will be released for the Kinetis in the next month or so, more info here http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EGUI&fsrch=1&sr=3

 

0 件の賞賛
返信
5,301件の閲覧回数
lyxljh
Contributor I

Hi, Freegeek,

 

    Thank you very much for your reply.

 

    Would you please tell me when MQX will be integrated with Codewarrior supporting K60? And what's the ultimated   date that eGUI will be released for the Kinetis?

 

    Thanks!

 

 

0 件の賞賛
返信
5,301件の閲覧回数
mnorman
NXP Employee
NXP Employee

Michael,

 

We expect MQX 3.7 with Kinetis CodeWarrior support and the release of eGUI with MQX and Kinetis support to both be available by the first week of April.

 

-mnorman4

0 件の賞賛
返信
5,301件の閲覧回数
lyxljh
Contributor I

Good news. Hope it available ASAP.

Thank you very much, mnorman4!

0 件の賞賛
返信
5,301件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

See also the following: http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf

Note that there is a problem with the Flexbus sharing with IR interface on the first Kinetis tower boards, which otherwise stops the TFT from working - the workaround is explained in the document.

Also see the TFT display operating here: http://www.youtube.com/watch?v=AdtRyQ-2IrE (this is with Kirin3 board but the Kinetis does the same)

 

Regards

 

Mark

 

0 件の賞賛
返信
5,301件の閲覧回数
lyxljh
Contributor I

Mark,

 

    Thanks a lot for your reminding.

 

    I have found the explanation in the document, and will study further.

 

    Have a nice day!

0 件の賞賛
返信