Kinetis USB Boot ROM - Now or Planned?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis USB Boot ROM - Now or Planned?

1,281 Views
dvona
Contributor II


I'm curious if Freescale has any plans to include a Boot ROM that supports the USB device mode on many of the parts in the kinetis portfolio.  Specifically, something akin to the EZ Port, but for USB.

I understand there is code available that can be programmed into flash, but I am looking for a solution for a new part without resident code.  I do not see anything in the existing portfolio today.

Regards,

-Dan

0 Kudos
Reply
1 Reply

1,105 Views
perlam_i_au
Senior Contributor I

I am afraid that option has not been announced yet, nor even as possibility.


Cheers,
Perla

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply