Kinetis USB Boot ROM - Now or Planned?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis USB Boot ROM - Now or Planned?

1,258件の閲覧回数
dvona
Contributor II


I'm curious if Freescale has any plans to include a Boot ROM that supports the USB device mode on many of the parts in the kinetis portfolio.  Specifically, something akin to the EZ Port, but for USB.

I understand there is code available that can be programmed into flash, but I am looking for a solution for a new part without resident code.  I do not see anything in the existing portfolio today.

Regards,

-Dan

ラベル(3)
0 件の賞賛
返信
1 返信

1,082件の閲覧回数
perlam_i_au
Senior Contributor I

I am afraid that option has not been announced yet, nor even as possibility.


Cheers,
Perla

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信