Hi All,
I have a problem with Kinetis MKL24 based device.
It is powered with a single cell 3.0 V battery.
My software project is build with Processor Expert drivers, including MQX Lite OS driver.
I have a very simple single task that loops every 1 second and blinks some LED.
For some reason around 50% of cases when I insert battery into a socket my device does not start (no LED blinking).
I found that if I short-circuit GND with RESET pins on PCB's programming socket for a moment it starts do blink.
It also starts every time when started from under debugger.
Do you have any ideas what's the problem?
 
					
				
		
I managed to dig deeper into the problem.
I found out that when my application does not start it is because MCU is entering Low Power Wait mode.
I have not enabled any of power saving options available in ProcessorExpert yet but I see that it is executing "wfi" command (line 46):
ASM_PUBLIC_BEGIN(_sched_execute_scheduler_internal)
ASM_PUBLIC_FUNC(_sched_execute_scheduler_internal)
ASM_LABEL(_sched_execute_scheduler_internal)
#if MQX_ENABLE_USER_MODE
cpsid i
push {r0}
mrs r0, IPSR
cmp r0, #0xb
pop {r0}
bne _sched_execute_scheduler_internal2
push {lr}
//bl _set_pend_sv
cpsie i
pop {pc}
ASM_LABEL(_sched_execute_scheduler_internal2)
cpsie i
#endif
// store active task registers
STORE_ALL_REGISTERS
// disable interrupts
cpsid i
GET_KERNEL_DATA r0
ldr r3, [r0, #KD_ACTIVE_PTR] // get active task descriptor
str r1, [r3, #TD_STACK_PTR] // store task SP to task descriptor td
#if MQX_KERNEL_LOGGING
KLOG r0, ASM_PREFIX(_klog_execute_scheduler_internal) // kernel log this function
#endif
ASM_LABEL(sched_internal)
ldr r1, [r0, #KD_CURRENT_READY_Q] // get current ready q
ASM_LABEL(find_noempty_que)
ldr r2, [r1, #0] // address of first td
cmp r2, r1 // ready_q structure itself?
bne switch_task
ldr r1, [r1, #RQ_NEXT_Q] // try next queue
movs r1, r1
bne find_noempty_que
// r1 is 0 -> empty
ASM_LABEL(no_one_to_run)
// wait for interrupt
cpsie i
wfi
cpsid i
// TODO check r0, must be kernel data
ldr r1, [r0, #KD_READY_Q_LIST] // get first que from ready list
b find_noempty_que
ASM_LABEL(switch_task)
// update kernel structures
str r1, [r0, #KD_CURRENT_READY_Q] // store addr for active que
str r2, [r0, #KD_ACTIVE_PTR] // active task descriptor
ldrh r3, [r2, #TD_TASK_SR]
strh r3, [r0, #KD_ACTIVE_SR] // restore priority mask for enabled interrupt for active task
Any ideas what and why is hapenning?
 
					
				
		
Ok, found some more again :smileyhappy: ...
I have 32kHz generator connected to RTC_CLKIN pin.
I also have ProcessorExpert's RTC_LDD component added. Its clock source is set to ERCLK32K.
In CPU bean's option for RTC Clock input is enabled.
The problem appears when this RTC component has its interrupts options enabled (INT_RTC and INT_RTC_Seconds interrupts).
When these interrupts are disabled my MCU starts with no Low Power Wait.