Kinetis MK70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,390件の閲覧回数
Microfelix
Contributor IV

Hi,

I developed a project with Kinetis PK70 to 120MHz.

I'm going through the production with the Kinetis MK70 up to 150MHz.

Wondering if the firmware developed with CodeWarrior 10.3 and MQX 3.8, are compatible or need to change the setting to run MK70.

thanks

Maurizio

ラベル(1)
1 解決策
2,086件の閲覧回数
apanecatl
Senior Contributor II

Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.

元の投稿で解決策を見る

2 返答(返信)
2,087件の閲覧回数
apanecatl
Senior Contributor II

Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.

2,086件の閲覧回数
monXii
Contributor III

hello.

is there a new BSP for the MK70 ?

have the same problem .. we are using the MQX ..

0 件の賞賛
返信