Kinetis MK70

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis MK70

跳至解决方案
1,519 次查看
Microfelix
Contributor IV

Hi,

I developed a project with Kinetis PK70 to 120MHz.

I'm going through the production with the Kinetis MK70 up to 150MHz.

Wondering if the firmware developed with CodeWarrior 10.3 and MQX 3.8, are compatible or need to change the setting to run MK70.

thanks

Maurizio

标签 (1)
1 解答
1,215 次查看
apanecatl
Senior Contributor II

Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.

在原帖中查看解决方案

2 回复数
1,216 次查看
apanecatl
Senior Contributor II

Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.

1,215 次查看
monXii
Contributor III

hello.

is there a new BSP for the MK70 ?

have the same problem .. we are using the MQX ..

0 项奖励
回复