Kinetis MK70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis MK70

Jump to solution
2,242 Views
Microfelix
Contributor IV

Hi,

I developed a project with Kinetis PK70 to 120MHz.

I'm going through the production with the Kinetis MK70 up to 150MHz.

Wondering if the firmware developed with CodeWarrior 10.3 and MQX 3.8, are compatible or need to change the setting to run MK70.

thanks

Maurizio

Labels (1)
1 Solution
1,938 Views
apanecatl
Senior Contributor II

Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.

View solution in original post

2 Replies
1,939 Views
apanecatl
Senior Contributor II

Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.

1,938 Views
monXii
Contributor III

hello.

is there a new BSP for the MK70 ?

have the same problem .. we are using the MQX ..

0 Kudos
Reply