Kinetis L Flash retention lifespan

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis L Flash retention lifespan

ソリューションへジャンプ
2,819件の閲覧回数
GordyCarlson
NXP Employee
NXP Employee

  My customer seeks confirmation that a user program that has been programmed once (or perhaps twice) into Kinetis KL04 flash will be retained in flash for 10 years.  We are not seeking an endurance number (ie....using Flash like EE for many writes)..... just a level of confidence that the original user program in Kinetis KL04 flash will be retained for 10 years.

Gordy Carlson

Freescale FAE

Upstate NY

ラベル(1)
0 件の賞賛
返信
1 解決策
2,521件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Gordon,

Below KL04 Flash specification about reliability is for normal flash operation and retention life:

flash.png

For KL04 doesn't have FlexNVM feature, which could bring confusion to customer.

In fact, the NVM here is nonvolatile memory abbreviation, which is no means FlexNVM.

Wish it helps.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,522件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Gordon,

Below KL04 Flash specification about reliability is for normal flash operation and retention life:

flash.png

For KL04 doesn't have FlexNVM feature, which could bring confusion to customer.

In fact, the NVM here is nonvolatile memory abbreviation, which is no means FlexNVM.

Wish it helps.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,521件の閲覧回数
johntaylor
Contributor I

Hello Ma Hui,

A few related questions:

1) What does "cycling endurance" mean?  What happens after 10k cycles?  Does the memory cell fail to retain the value?

2) Do reads affect the endurance?

3) Is this spec for a single cell, or does this apply to a sector or block of memory?  For example, if the memory is segmented into 1024 bytes does a write to byte 0 and a write to byte 1 count as 1 write in each cell, or 2 writes?

4) Is it reasonable to follow the "curve" and say that after 100k cycles we could expect a minimum of 0.5 years of data retention?

Thanks!

JT

0 件の賞賛
返信
2,521件の閲覧回数
GordyCarlson
NXP Employee
NXP Employee

Thank You!  Perfect

-Gordy

0 件の賞賛
返信