Kinetis KV4x - enabling clock output on the CLKOUT pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis KV4x - enabling clock output on the CLKOUT pin

1,530 次查看
nariane
Contributor I

I'm trying to enable clock output on the CLKOUT pin while running the microcontroller in "High-Frequency, High-Gain" mode.

To enable this output, I configured the microcontroller as follows:

1) I enabled the CLKOUT pin

 

// enables CLKOUT alternate function on pin PTC3
CLOCK_EnableClock(kCLOCK_PortC);
PORT_SetPinMux(PORTC, 3U, kPORT_MuxAlt5);

 

2) I enabled the external reference clock on the CLKOUT pin

 

OSC->CR |= OSC_CR_ERCLKEN(1); // enables OSCERCLK)
SIM->SOPT2 |= SIM_SOPT2_CLKOUTSEL(6); // CLKOUTSEL = OSCERCLK

 

I'm not able to measure anything on the CLKOUT pin, am I missing something? The same configuration shown above works if I configure the microcontroller in "High-Frequency, Low-Power Mode": in this case I'm able to measure the clock waveform on CLKOUT pin.

(my application works without problems in both "low power" and "high gain" modes)

Thanks for your help.

 

标签 (1)
0 项奖励
回复
1 回复

1,487 次查看
nariane
Contributor I

I managed to solve my problem by dividing the frequency of OSCERCLK by 2

// Divide OSCERCLK clock frequency by 2
OSC->DIV &= ~(OSC_DIV_ERPS_MASK);
OSC->DIV |= OSC_DIV_ERPS(1);

Apparently the clock frequency was too high (10Mhz); if I lower it to 5Mhz it works even in high gain mode.

0 项奖励
回复