Kinetis KL15 PIT interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KL15 PIT interrupt

1,990 Views
chobin
Contributor III

Dear Sirs,

I'm working with kinetis KL15 and I need to use the PIT peripheral. I configured it using the processor expert (I enclosed it).

I inserted the interrupt PIT function, but the code doesn't fall in it. I verified the interrupt flag of each channel and they are set  correctly by the microcontroller.

Have you got any idea to solve this problem?

Please, let me know.

Many thanks in advance for your support.

Best Regards,

Stefano

0 Kudos
Reply
1 Reply

1,892 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Chobin,

I was wondering if you can share your demo, then it would help me to figure out the issue by have a look through the code.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply