Kinetis KL05 clock configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis KL05 clock configuration

2,114件の閲覧回数
juanm
Contributor III


Hi! I have a custom board with a KL05, 32 pin LQFP package, and an 8 MHz crystal. I also have the sample code package available from NXP website and I'm trying to use the files mcg.c and mcg.h in order to get a 48 MHz clock frequency.

I'm using the function fei_fee(). I understand that this function allows me to go from the default fei mode to the fee mode.

But I'm having troubles with this. If I use it like this:

clk = fei_fee(8000000,LOW_POWER,CRYSTAL);

The returned value is 20000000 (20 MHz), so I would like to know what function I need to use in order to get a 48 MHz clock from the 8 MHz external crystal.

Thanks!

PS: I'm using the last version of the Kinetis Design Studio and I don't want to use processor expert for this.

0 件の賞賛
返信
1 返信

1,662件の閲覧回数
juanm
Contributor III

Anyone?

0 件の賞賛
返信