Kinetis K70 and 8-bit NAND Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K70 and 8-bit NAND Flash

Jump to solution
3,519 Views
andreyvarsegov
Contributor I

Hi,

I can not find the documentation for the connection diagram via NFC and 8-bit NAND Flash chip.

How to connect the data bus ?  In 8-bit mode used NFC_D0-NFC_D7 or NFC_D8-NFC_D15?

NFC_D0 - NAND_D0

...

NFC_D7 - NAND_D7

or

NFC_D8 - NAND_D0

...

NFC_D15 - NAND_D7

Best regards, Andrey.

Labels (1)
Tags (5)
0 Kudos
Reply
1 Solution
3,150 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrey

Sorry, I think as Flexbus by mistake.You should connect low data bus. Please reference attached picture.8-bit NFC.jpg

Best Regards

Paul

View solution in original post

0 Kudos
Reply
5 Replies
3,150 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrey

You can connect to FB_D0 - FB_D7.

0 Kudos
Reply
3,150 Views
andreyvarsegov
Contributor I

Thank you for quick answer, but you sure to FB_D0 - FB_D7 ? May be NFC_DATA0 - NFC_DATA7, because at TWR-K70F120M-SCH.pdf  16-bit NAND Flash connected to NFC_DATA0-DATA15, not to FB_D0-D15.

Best regards, Andrey.

0 Kudos
Reply
3,150 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Andrey,

In NFC 8-bit mode, please connect  NFC_D0-NFC_D7 with external 8-bit NAND Flash device.

Wish it helps.

3,150 Views
andreyvarsegov
Contributor I

Hi Hui_Ma,

Thank you very match!

Best regards, Andrey.

0 Kudos
Reply
3,151 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrey

Sorry, I think as Flexbus by mistake.You should connect low data bus. Please reference attached picture.8-bit NFC.jpg

Best Regards

Paul

0 Kudos
Reply