Kinetis K66 conflicting documents

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K66 conflicting documents

1,288件の閲覧回数
working1
Contributor I

Hi, 

I am referring to document BRKINETISSECSOLS REV3 and K66P144M180SF5RMV2.

They are highly conflicting: according to the first document K66 has neither hardware crypto support, nor memory protection unit.  But in the reference manual of K66, both are listed.

Which statement is correct? Are there differences in the various K6x memory protection units? Could it be that the first document is completely missleading?

Thank you for answers!

ラベル(2)
0 件の賞賛
返信
1 返信

1,177件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Of course, the K66P144M180SF5RMV2 is correct and official, the description in BRKINETISSECSOLS is inaccurate, there is not difference for the MPU for K66 family. pls refer to K66P144M180SF5RMV2.

Hope it can help you

BR

Xiangjun Rong