Kinetis K64F /K66F code licence for SDCard/MMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis K64F /K66F code licence for SDCard/MMC

跳至解决方案
2,621 次查看
mahendranmanoha
Contributor III

Hi,

I am planning to use the sample code in my small project from KSDK example projects such as "usb_examples_dev_msc_sdcard_bm".

I am wondering if this code is generic to both SD and MMC card or does this code also contains SDCard specific licensed code.

In simple terms, do I need to pay a license fee if I use this code?

best regards,

Mahendran.

标记 (4)
1 解答
2,471 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mahendran,

   All the code in the SDK which you downloaded from nxp official website, you can use it, it's no problem.

   If you just want to use the SD and MMC driver, not the usb code, I suggest you use the middleware driver, take K64 sdk as an example, you can find the sdmmc driver from this folder:

SDK_2.2_TWR-K64F120M\middleware\sdmmc_2.1.2

Please check you SDK package.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,472 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mahendran,

   All the code in the SDK which you downloaded from nxp official website, you can use it, it's no problem.

   If you just want to use the SD and MMC driver, not the usb code, I suggest you use the middleware driver, take K64 sdk as an example, you can find the sdmmc driver from this folder:

SDK_2.2_TWR-K64F120M\middleware\sdmmc_2.1.2

Please check you SDK package.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,471 次查看
mahendranmanoha
Contributor III

Thanks Kerry for the confirmation.

I am planning to use the SD Card code along with USB. So, I will use most of the code along with my application. 

I am glad that I do not need to pay for SD Card code that are used in K64 or K66 examples.

Thanks,

Mahendran.

0 项奖励
回复
2,471 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

You are welcome.

 All the SDK code which you can downloaded from our nxp website is free, feel free to use it.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复