Kinetis K64 Ref clock output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K64 Ref clock output

ソリューションへジャンプ
2,390件の閲覧回数
eduardrazumovsk
Contributor III

Hello,

Can i output a 24MHz clock from the MCU to other IC ? if so, what are the restrictions ?

MK64FN1M0VDC12 is connected to USB HUB, i want to save the cost of 24MHz crystal required by the USB HUB

Best Regards

1 解決策
2,219件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eduard Razumovsky:

It might be possible to use the FTM (FlexTimer) to get a 24 MHz clock. See these similar threads:

Re: Unable to get PWM to work with ext crystal-only configuration

Re: What components do I need to output PWM using FTM module by Processor Expert ?

How could I output 50MHz square waveform by using FRDM-K64F?

BUT, for a USB HUB this would be really not recommended. USB specifications and timings are very strict. So it should be of course better to use an oscillator or crystal.

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

2 返答(返信)
2,219件の閲覧回数
eduardrazumovsk
Contributor III

Thanks a lot Jorge

Regards

Eduard

0 件の賞賛
返信
2,220件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eduard Razumovsky:

It might be possible to use the FTM (FlexTimer) to get a 24 MHz clock. See these similar threads:

Re: Unable to get PWM to work with ext crystal-only configuration

Re: What components do I need to output PWM using FTM module by Processor Expert ?

How could I output 50MHz square waveform by using FRDM-K64F?

BUT, for a USB HUB this would be really not recommended. USB specifications and timings are very strict. So it should be of course better to use an oscillator or crystal.

Regards!

Jorge Gonzalez