Kinetis K60 and ISO7816

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K60 and ISO7816

ソリューションへジャンプ
3,429件の閲覧回数
SergeMaslenniko
Contributor II

Hi Everyone!

I need to connect two Smart-Cards to K60, UART0 and UART1 support ISO7816.

Smart-Card ISO7816 has CLK and I/O.

I/O is to be connected to appropriate UART-TX of the MCU in accordance with Reference Manual.

But where am I to connect CLK of Smart-Card?

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,545件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Serge

You can connect CLK to a flex timer output pin directly.

pastedImage_0.png

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,546件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Serge

You can connect CLK to a flex timer output pin directly.

pastedImage_0.png

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信
2,545件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Paul,

Do we have reference design, appnote, and/or example project for Kinetis doing ISO7816 support?

Customer looking for K60 or K64 level of capability.

Regards,

David

0 件の賞賛
返信
2,545件の閲覧回数
ND2
Contributor III

We are also looking for the same.

Trying to connect the KL27Z to the smart card J3D081 (https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf ). Just need to send the ATR and read the response over ISO7816. We have been able to get the same working on the LPC11U24 but even after spending considerable amount of time we have made much progress.

Thanks

Neel.

0 件の賞賛
返信