Kinetis K60 and ISO7816

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K60 and ISO7816

Jump to solution
3,430 Views
SergeMaslenniko
Contributor II

Hi Everyone!

I need to connect two Smart-Cards to K60, UART0 and UART1 support ISO7816.

Smart-Card ISO7816 has CLK and I/O.

I/O is to be connected to appropriate UART-TX of the MCU in accordance with Reference Manual.

But where am I to connect CLK of Smart-Card?

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Solution
2,546 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Serge

You can connect CLK to a flex timer output pin directly.

pastedImage_0.png

Hope my reply can help you.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
3 Replies
2,547 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Serge

You can connect CLK to a flex timer output pin directly.

pastedImage_0.png

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply
2,546 Views
DavidS
NXP Employee
NXP Employee

Hi Paul,

Do we have reference design, appnote, and/or example project for Kinetis doing ISO7816 support?

Customer looking for K60 or K64 level of capability.

Regards,

David

0 Kudos
Reply
2,546 Views
ND2
Contributor III

We are also looking for the same.

Trying to connect the KL27Z to the smart card J3D081 (https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf ). Just need to send the ATR and read the response over ISO7816. We have been able to get the same working on the LPC11U24 but even after spending considerable amount of time we have made much progress.

Thanks

Neel.

0 Kudos
Reply