Kinetis K40 Serial Card - COM Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K40 Serial Card - COM Issue

Jump to solution
1,667 Views
ignisuti
Contributor IV

I've defined SERIAL_CARD and undefined OSJTAG in the K40_tower.h file. However, I'm still unable to get data to output on my RS232 connector. 

 

I have the RS232 connector connected to cable which then connects to a Serial to USB adpter. That adapter is plugged into my computer's USB port. 

 

The funny thing is that I when I disconnect from the Tower Kit RS232 serial connector, I can connect to the COM port in HyperTerminal. When I reconnect to the RS2323 serial connector, I can no longer connect in Hyperterminal.

 

Suggestions please...

0 Kudos
Reply
1 Solution
1,466 Views
ignisuti
Contributor IV

I figured it out after looking at the user manual I found here: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRSERUM.pdf?fpsp=1

 

I moved jumper J16 from 1-2 to 3-4.

 

Also, the RS232 communication seems to only work when the tower kit is supplied with power from the programming card. If the tower is powered via the elevator card or the serial card, then the serial output does not work.

View solution in original post

0 Kudos
Reply
1 Reply
1,467 Views
ignisuti
Contributor IV

I figured it out after looking at the user manual I found here: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRSERUM.pdf?fpsp=1

 

I moved jumper J16 from 1-2 to 3-4.

 

Also, the RS232 communication seems to only work when the tower kit is supplied with power from the programming card. If the tower is powered via the elevator card or the serial card, then the serial output does not work.

0 Kudos
Reply