Kinetis K40 Serial Card - COM Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K40 Serial Card - COM Issue

ソリューションへジャンプ
1,720件の閲覧回数
ignisuti
Contributor IV

I've defined SERIAL_CARD and undefined OSJTAG in the K40_tower.h file. However, I'm still unable to get data to output on my RS232 connector. 

 

I have the RS232 connector connected to cable which then connects to a Serial to USB adpter. That adapter is plugged into my computer's USB port. 

 

The funny thing is that I when I disconnect from the Tower Kit RS232 serial connector, I can connect to the COM port in HyperTerminal. When I reconnect to the RS2323 serial connector, I can no longer connect in Hyperterminal.

 

Suggestions please...

0 件の賞賛
返信
1 解決策
1,519件の閲覧回数
ignisuti
Contributor IV

I figured it out after looking at the user manual I found here: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRSERUM.pdf?fpsp=1

 

I moved jumper J16 from 1-2 to 3-4.

 

Also, the RS232 communication seems to only work when the tower kit is supplied with power from the programming card. If the tower is powered via the elevator card or the serial card, then the serial output does not work.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,520件の閲覧回数
ignisuti
Contributor IV

I figured it out after looking at the user manual I found here: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRSERUM.pdf?fpsp=1

 

I moved jumper J16 from 1-2 to 3-4.

 

Also, the RS232 communication seems to only work when the tower kit is supplied with power from the programming card. If the tower is powered via the elevator card or the serial card, then the serial output does not work.

0 件の賞賛
返信