Kinetis K24 devices simulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K24 devices simulator

2,722件の閲覧回数
adamkoronowski
Contributor I

Hello,
I'm looking for simulator (or IDE with simulation option) for the Kinetis K24 devices. I want to execute unit tests on software simulation. Can anyone recommend me, a proven simulation solution (software application, IDE) with ability to redirect UARTs output to text file.

Adam

ラベル(1)
3 返答(返信)

2,458件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Adam,

Unfortunately NXP does not offer any simulator for the Kinetis family. There is also QEMU, I have not tried it but you could give it a try:

The GNU ARM Eclipse QEMU 

Please notice that this simulator is mostly core simulator and do not simulate the full device.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,458件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Fortunately uTasker does already include Kinetis simulation for (approx.) real-time simulation of almost all KE, KEA, KL, K, KV, (KW) parts - since 2011. It has been used for the development of hundreds of Kinetis based products and saves developers huge amounts of time, as well as getting Kinetis based products faster to market, with more reliable operation due to better development/debugging/testing/code reviews.

Are my posts pointing this out completely INVISIBLE to NXP????????????????

Rather frustrated regards

Mark

2,458件の閲覧回数
mjbcswitzerland
Specialist V

Hi

See http://www.utasker.com/kinetis/TWR-K24F120M.html

Works with VisualStudio IDE and cross-compiles to final target with GCC (or from KDS, CW, IAR, Keil, Green Hills, CooCox, Rowley, etc.).
Simulates Ports, interrupts, DMA, UARTs, USB, ADC, Timers (PITs, LPTR, SYSTICK, PDB, RTC, FlexTimer), Low Power wakeups, Ethernet, CAN, Flash, I2C, SPI, SDHC, SPI, keyboards.

UART output is saved to a file and also sent to PC COM ports (or COM loop backs) so that the simulation of UART based applications can be connected to other devices for real-time operation.

Complete project simulation in (approx.) real-time to test and debug final code in the environment to eliminate most target debugging requirements. Project develpment times with it are greatly reduced over traditional methods.

Most KEA, KE, KL, K, KV etc. Kinetis parts are supported and projects developed for one type can operate on most other types with no (or only minor) porting effort.

Regards

Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html